Viewing Disturbance Direction
View Disturbance Direction to analyze the likely origin of voltage disturbance events in your power system.
NOTE: Disturbance Direction analysis is only available for alarm instances and incidents, not for alarm status. Also, the data associated with the alarm or incident must include disturbance direction information.
To view Disturbance Direction:
- In the alarm viewer, open an existing alarm history or incident history view from the view library or add a new View.
TIP: Add a Disturbance Direction filter to your view to identify disturbance direction relevant alarms and incidents. You can add this filter in View Settings > Categories > Power Quality.
NOTE: The Disturbance Direction filter settings only apply to the following Power Quality alarm or incident types: Interruption, Under Voltage, Over Voltage, Sag, Swell, Unclassified Disturbance, Transient.
 - Find the alarm instance or Incident  for which you want to view Disturbance Direction and click Open Details
 to open the details window.TIP: Alarms or incidents with Disturbance Direction information are tagged with an Upsteam
 or Downstream 
 indicator. - In the details window, view the Disturbance Direction information of the representative disturbance for this alarm or incident.
 
Related topics:
- Viewing incidents
 - Viewing alarms
 - Viewing events
 - Viewing Disturbance Direction
 - Viewing Load Impact
 - Viewing a timeline analysis
 - Viewing Voltage Tolerance
 - Viewing waveforms
 - Acknowledging alarms
 
For reference information see:
- Alarm Operation
 - Incidents
 - Alarms
 - Events
 - Disturbance Direction
 - Load Impact
 - Timeline analysis
 - Voltage Tolerance
 - Waveforms
 - Waveform analytics
 - Alarms terminology
 - Alarms UI
 - Timeline analysis UI
 - Waveforms UI
 
For information on how to configure Alarms, see Alarms configuration.