Viewing waveforms
View waveforms to investigate power quality events and identify root causes of disturbances.
To view waveforms:
- In the alarm viewer, open an existing Incident history view or alarm history view from the view library or add a new View.
 - Find the incident or alarm for which you want to view waveforms and click Details 
 .  You can also open Details by double-clicking the incident or alarm instance. - In Details, click Waveforms.
TIP: Click Open Representative Waveform to see the representative waveform for this Incident or alarm instance.
 - View the waveforms associated with the incident or alarm instance.
(Optional) Click Inspect a waveform to see more details and to analyze the waveform.
 
Related topics:
- Viewing incidents
 - Viewing alarms
 - Viewing events
 - Viewing Disturbance Direction
 - Viewing Load Impact
 - Viewing a timeline analysis
 - Viewing Voltage Tolerance
 - Viewing waveforms
 - Acknowledging alarms
 
For reference information see:
- Alarm Operation
 - Incidents
 - Alarms
 - Events
 - Disturbance Direction
 - Load Impact
 - Timeline analysis
 - Voltage Tolerance
 - Waveforms
 - Waveform analytics
 - Alarms terminology
 - Alarms UI
 - Timeline analysis UI
 - Waveforms UI
 
For information on how to configure Alarms, see Alarms configuration.