Viewing events
View events to investigate system activities in PME or to troubleshoot unexpected system behavior.
To view events:
- In the alarm viewer, open an existing event view from the view library or add a new View.
 - View the event Information displayed in the alarms display pane.
(Optional) In the view Library, right-click the view name or click Options
 for this view and select Edit to open the view settings.  You can also open the view settings by double-clicking the view name. Adjust the  settings for  View Type, Priority and Sources to customize the view if necessary. Save the modified view settings or click Cancel to discard the changes. 
TIP: Double-clicking an event in the events display table opens the associated alarm.
Related topics:
- Viewing incidents
 - Viewing alarms
 - Viewing events
 - Viewing Disturbance Direction
 - Viewing Load Impact
 - Viewing a timeline analysis
 - Viewing Voltage Tolerance
 - Viewing waveforms
 - Acknowledging alarms
 
For reference information see:
- Alarm Operation
 - Incidents
 - Alarms
 - Events
 - Disturbance Direction
 - Load Impact
 - Timeline analysis
 - Voltage Tolerance
 - Waveforms
 - Waveform analytics
 - Alarms terminology
 - Alarms UI
 - Timeline analysis UI
 - Waveforms UI
 
For information on how to configure Alarms, see Alarms configuration.