Viewing Load Impact
View Load Impact to identify changes in steady state electrical loads in your power system triggered by a voltage disturbance.
NOTE: Load Impact analysis is only available for alarm instances and incidents, not for alarm status. Also, the data associated with the alarm or incident must meet the prerequisites. See Load Impact for more information.
To view Load Impact:
- In the alarm viewer, open an existing alarm history or incident history view from the view library or add a new View.
TIP: Add a Load Impact filter to your view to identify load impact relevant alarms and incidents. You can add this filter in View Settings > Categories > Power Quality.
NOTE: The Load Impact filter settings only apply to the following Power Quality alarm or incident types: Interruption, Under Voltage, Over Voltage, Sag, Swell, Unclassified Disturbance, Transient.
 - Find the alarm instance or Incident  for which you want to view Load Impact and click Open Details
 to open the details window.TIP: Alarms or incidents with Load Impact calculations are tagged with a Load Loss
 or Load Gain 
 label. You can enable or disable the display of the label in Web Applications > Settings > Alarms > Alarm Views.  - In the details window, view the Load Impact information related to this alarm or incident.
TIP: See Load Impact calculations for more details.
 
Related topics:
- Viewing incidents
 - Viewing alarms
 - Viewing events
 - Viewing Disturbance Direction
 - Viewing Load Impact
 - Viewing a timeline analysis
 - Viewing Voltage Tolerance
 - Viewing waveforms
 - Acknowledging alarms
 
For reference information see:
- Alarm Operation
 - Incidents
 - Alarms
 - Events
 - Disturbance Direction
 - Load Impact
 - Timeline analysis
 - Voltage Tolerance
 - Waveforms
 - Waveform analytics
 - Alarms terminology
 - Alarms UI
 - Timeline analysis UI
 - Waveforms UI
 
For information on how to configure Alarms, see Alarms configuration.